STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Custome board with stm32f427 USB failure

Posted on April 23, 2018 at 13:28Hi,I am developing a custome board with the stm32f427.I cannot get the USB to connect to the PC. I allways get the number 43 error 'USB device unknown'The builtin bootloader is loaded and I can see the code running o...

Design for stm32f7 to programming

Posted on May 30, 2018 at 05:45Hi ! I have designed a board with stm32f765 (LQFP100) but I got a problem with it when I test this board. I connect the board through usb cable with st link v2 and the ST Link Utility can detect this stm32f7 but when I...

0690X00000604TbQAI.jpg

Some question about DWT working on the stm32F767

Posted on May 30, 2018 at 03:57I am using the STM32F7-Discovery board and have been stuck at trying to enable the DWT cycle ,From what I've seen online this should suffice for enabling it:#define DWT_CR *((volatile unsigned int *)0xE0001000)#define ...

ADC DMA and injected mode

Posted on May 30, 2018 at 09:43Hi all, I am using a board with and STM32L476. ADC 1 is used in software triggered mode, with DMA (8 channels). (So firmware dictates when to start conversion, DMA interrupt tells the firmware to process the data.) Thi...

CAN Node not able to transmit when on an existing bus

Posted on May 25, 2018 at 09:34Hello Everyone,I,am having a issue with my can node.The communication bw two can nodes built on STM32L4 works perfectly fine. But that's just for testing purpose. I don't intend to use it that way.When I introduce it t...

Executing the program in SDRAM

Posted on May 26, 2018 at 11:57Hello! I'm using stm32f746igt. You can run the program in sdram on this controller and use Chrome Art to display the image on the display.

9-bit UART receive STM32F103

Posted on May 07, 2018 at 11:34Hello all,I am really new at all this, I hope someone has a simple example to help.I am trying to receive 9-bit data using the STM32-F103 in normal polling mode example code belowuint16_t messages[30]; HAL_UART_Receive...

STM32F407 RTC Daylight Savings bug or feature?

Posted on May 28, 2018 at 23:06I'm currently trying to sync the clock on my STM32F407 using the time from an NTP time server. The time server always responds in UTC time format without any daylight savings whatsoever. So I tried using the ADD1H bit ...

dave23 by Associate II
  • 2812 Views
  • 2 replies
  • 0 kudos

STM32L4 & CubeMX 4.25 clocksettings failure

Posted on April 26, 2018 at 19:04Hello All,I am using STM32L486RGT, CubeMX 4.25 STM32L4 lib 1.11.At the STM32 I have a 16MHz crystall connected.Now I run into problems setting up the clocktree. It works under certain combinations but not under the o...

taraben by Senior
  • 12782 Views
  • 17 replies
  • 1 kudos