User Activity

Hello,Can someone please provide a working download file for "STM32Cube function pack for STEVAL-PROTEUS1 sensor datalog and file transfer over BLE and USB"?The ZIP-File Version 1.1.0 is corrupt.It cannot be extracted neither on Windows, Linux or Mac...
I tried all 3 available demos: default, FP-AI and Datalogger.At last I flashed the original default demo back. All tests are done USB-powered or with LiPo.Establishing a BLE connection with iPhone works in 10% of the cases.Using an Android smartphone...
Hello.I have a small fan at home with STEVAL-MKI245A attached and STEVAL-MKI109V3 is near the fan as well,like you would using PROTEUS1.The fan offers 3 mechanical switches to modify the speed.Using the switches causes a stop of reading data from the...
libncurses5 and libtinfo5 were replaced by libncurses6 and libtinfo6 in Ubuntu 23.10.No Debug possible anymore inside IDE.Update not yet available.Is it safe to replace version 11.3 of the toolchain with i.e. 13.2?Will it work to overwrite the plugin...
1.) HAL_Delay(x) hangs forever when restarting CM4 using Hardware Timer for Systick. Every unit was forced with RESET/RELEASE. Any firmware change could not solve it. Have to repower the board. Happens in Normal and Engineering mode!2.) HAL_Init() ha...
Kudos from
Kudos given to