STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Uart output not coming as desired

Posted on May 28, 2018 at 14:31Hi,  am using STM32F103C8T6, I wrote code with keil for uart1 for the tx pin PA9 and rx pin PA10, am just sending a character repeatedly, but I didn't receive the character what I am sending, I am using CP2102 device b...

0690X0000060KyNQAU.png

Why does STM32CubeMX hang up on windows10 System?

Posted on May 14, 2018 at 16:34I use STM32CubeMX to create startup code for the STM32L433RCT-P (Nucleo-Board).On my old Windows7 system there was no problem generating the startup code but on the new Windows 10 system it stalls after(?) it copied th...

USB CDC or USART (with or except using printf) problem when using 1 seconds timer to output DAC(external DAC)

Posted on May 28, 2018 at 09:58Hello,I need your help to recognize my issue correctly, please help me,issue :when using timer as 1 second period to control main flow including printf output,and at that time if using another timer to control the outp...

STM32F030F4P STOP mode: enter and exit

Posted on November 14, 2017 at 22:09 Hello. I'm having some problems with the STOP mode of STM32F030F4P. After having all my application working with standbye mode awake by the RTC alarm, I checked that my application can not have...

CAN message reception without callbacks

Posted on May 24, 2018 at 15:52Hi All,I am currently developing an application using CAN1 with CMSIS driver on a STM32F413 controller. As the reception of CAN messages is not so time critical like other parts in the application, I wanted to poll man...

STM32 Ethernet Port (TCP Throughput)

Posted on May 28, 2018 at 12:09Hi Guys,I am currently performing the TCP throughput Test by using lwiperf framework as provided. I have performed the test on below Nucleo 144 pins board, NUCLEO-F207ZGNUCLEO-F746ZGBoth of the boards are running a mo...

0690X0000060KuHQAU.png 0690X0000060KuIQAU.png
whwong84 by Associate II
  • 1021 Views
  • 0 replies
  • 0 kudos

Mass storage problem with SD card

Posted on May 28, 2018 at 09:52Hello, i am trying to use the mass storage interface with my SD card by the help of the stm32 cube. My mcu is stm32f405 and i'm using SDIO 4 bits + USB full speed stack. I am able to see the device and read all the fil...

issa by Associate II
  • 736 Views
  • 0 replies
  • 0 kudos