STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

An error in the reference manual for STM32L4?

Posted on June 15, 2018 at 01:26I think there is an error In http://www.st.com/content/ccc/resource/technical/document/reference_manual/02/35/09/0c/4f/f7/40/03/DM00083560.pdf/files/DM00083560.pdf/jcr:content/translations/en.DM00083560.pdf. In figure...

M. Jeong by Associate II
  • 1540 Views
  • 2 replies
  • 0 kudos

How to know if it is necessary a Rext in HSE crystal?

Posted on June 26, 2018 at 11:19Hi everyone,I'm working on an STM32F1 platform. I'm using this crystal ABMM2-8.000MHZ-E2-T for the HSE setting.I made of the calculation according to the application note AN2867:According to the datasheet ABMM2-8.000M...

RTC Year?

Posted on June 23, 2018 at 02:06 Hi, Why the RTC Year is a uint8_t and value must be b/w 0 and 99? How do we map to real year? Thx /** * @brief RTC Date structure definition */ typedef struct { uint8_t WeekDay; /*!< Specifies the RTC D...

I2C Master Clock Stretching STM32F746

Posted on June 26, 2018 at 08:29I am experiencing a strange problem with the Clock stretching and the STM32f746. The STM is Bus Master and the slave is a MCP9600 that requires clock stretching.The data sheet of the MCP requires 60us stretching.Using...

ferrario by Associate III
  • 735 Views
  • 0 replies
  • 0 kudos

STM32 USART Additional features?

Posted on June 26, 2018 at 08:17Using STM32F0xx USART to communicate simplex in standard asynchronous mode (8 bits + parity) with many STM32F0xx slaves. Want to use additional USART features. Did understand and can use Idle and Break detection.What ...

JuM by Senior
  • 557 Views
  • 0 replies
  • 0 kudos

stm32f1 UART and CDC works same for receiving string inside mcu single char receive store in buffer and so on til end char

Posted on June 26, 2018 at 04:07in programming stm32f103cbt6 how can i receive complete string in mcu  send by pc using VCP driver?uart recive char store in buffer so on till end char same process for cdc receive string data?or any other solution fo...

Problem with STEVAL- IHP007V1

Posted on June 26, 2018 at 04:05I have two problem with  STEVAL- IHP007V11. I can't  find pin of connector in schematic of this evaluation board here https://www.st.com/resource/en/schematic_pack/steval-ihp007v1_schematic.pdf 2. User manual of STEVA...

0690X0000060LTaQAM.png
Hung Le by Associate
  • 721 Views
  • 0 replies
  • 0 kudos