STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Porting code from STM32 Nucleo (F103RB) to STM32F103VG

Posted on June 25, 2018 at 18:13Hi, I am having an issue when I try to load code to my STM32F103VG device over the KEIL interface.I have written code for the STM32 Nucleo-64 board which contains #STM32F103RBT6 device and it works without any issue. ...

daithi62 by Associate II
  • 2110 Views
  • 2 replies
  • 0 kudos

Minor bug in USART documentation

Posted on June 26, 2018 at 18:29''Figure 1'' here:should probably be ''Figure 279. USART block diagram''.I see the same mistake in RM0090 rev.17, so this will be probably across several RMs.JW[EDIT] Textual search for ''Figure 1'' brought up also th...

0690X0000060LUJQA2.png 0690X0000060LUTQA2.png

Can't send CAN message - Mailboxes always full

Posted on June 25, 2018 at 17:34 Hello, I'm trying to configure the CAN-bus peripheral in loopback mode so I can later develop a real network. I'm using the Nucleo L432KC board and my clock is 32MHz. My problem is that I can't send any mess...

STM32 BOOTLOADER [UART]

Posted on June 25, 2018 at 12:22I know this question was asked many times before me, but its still a lot of info which is hard to find. My mcu is stm32f407, what im trying to do is be able to load firmware to mcu thourgh PC, im plannig to use Visual...

3MHZ pulse counter with trigger output

Posted on June 23, 2018 at 13:27Hi, i'm totaly new to stm32 actually i have been looking for a solution to test some motion control output the case is:i need to measure number of pulse that motion give it at speed of around 3mhz and when the number ...

SPI-MicroSD card adapter

Posted on June 26, 2018 at 07:48I just started working on this device and I wish to interface it with an STM32F446RE board. I saw in a number of other threads that using the stm32_adafruit_sd.c was an easy way to use this. There are also a number of...

STM32H743 dual ADC w DMA

Posted on June 21, 2018 at 11:37The original post was too long to process during our migration. Please click on the attachment to read the original post.

STM32L152 recieves garbage via USART3

Posted on June 25, 2018 at 13:33Hi,I am new to STM32 and  using the STM32L152 to transmit and receive characters via USART. I can transmit data with no problem but when i want to recieve data using the Hterminal, the mcu always gets an extra charact...