STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Writing multiple blocks to SD card fails

Posted on August 02, 2017 at 14:19Hello. I am developing application that involves writing multiple blocks (of 512 bytes) to SD card. It is a part of USB MSC application, multiblock operations are required for correct and fast functioning. A BSP_SD_...

Ivan Ivan by Associate II
  • 1933 Views
  • 3 replies
  • 0 kudos

stm32 I2C3 master: wont transfer data

Posted on June 26, 2018 at 00:02I am having difficulty transmitting on my stm32l071k8. I am using a STM32l073RZ nucleo board for benchtop development.my lab setup is just a nucleo board connected to an oscilloscope for SCL and SDA. Currently my devi...

Resolved! USB Host on USB-IF Compliance Program

Posted on June 22, 2018 at 01:44Hello,We implemented USB Host on a product based on STM32F427 MCU. Now we try to test it on USB-IF compliance program. But it fails to satisfy the USB-IF requirements.Questions we have:1. Does USB Host support USB Hub...

Pilot B by Associate II
  • 1955 Views
  • 2 replies
  • 0 kudos

Did I break my 407 with +5V?

Posted on June 26, 2018 at 01:12I accidentally used a 5V regulator instead of 3.3V. After fixing that the SWD dongle/ST link says no connection to target. This happens to be my only prototype now. Building a new or swapping the 100pin STM32F407 isn'...

LMI2 by Lead
  • 1024 Views
  • 1 replies
  • 0 kudos

I2C issue with STM32H7 MCU

Posted on June 11, 2018 at 19:14Hello.,., I am using STM32H7 newly released MCU in our project,  In this 3 slave devices are connected thorough I2C interface (Audio codec,EEPROM,RTC devices), All slave devices are accessible and working fine with ro...

Sensortile UART pins 6 &7

Posted on June 19, 2018 at 23:32Hello,I'd like to use the UART pins on the SensorTile to receive data from another microcontroller (STM M0) via UART.  I've noticed all virtual com port examples for this device use the USBD library instead of UART li...

Steven Wu by Associate II
  • 1516 Views
  • 2 replies
  • 0 kudos

How to enable FPU in STM32F7

Posted on June 25, 2018 at 14:13I wanted to use FPU in STM32F7, How to enable FPU.Also how to check if it gets enabled?Majerle.Tilen.001 #stm32f7-nucleo #fpu

pjn by Associate II
  • 3392 Views
  • 3 replies
  • 0 kudos

stm32l476g-discovery kit demo program

Posted on June 25, 2018 at 15:57I tried flashing the kit with it's demo program with the demo ST provided.There's audo record function where i tried recording and playback all i heard is the noise.. Is it just me or anyone else ?Any fix for this ? #...

How to execute code from external flash on STM32F407

Posted on June 15, 2018 at 12:15 Hi, I have read the AN4852 application note explaining how to program an external QSPI flash using the built-in UART bootloader. However it does not tell how to execute afterwards the code saved in the external flas...

low accuracy for ADC1 on STM32F030R8-Nucleo

Posted on June 09, 2018 at 14:28Hey Guys,I am using the ADC1 to sample A0 as a voltage input and A17 and A18 as temperature and VrefInt for Temperature and exact Vdda calculaion. So far my implementation works fine. I also calibrate the ADC everytim...