cancel
Showing results for 
Search instead for 
Did you mean: 

stm32L496ZG dual boot

ron23
Associate
Posted on March 24, 2018 at 22:22

hi

im trying to implement dual boot using BFB2 bank switching on this chip, and after the code is burned in the second bank (ox80800000), it doesnt boot.

i single stepped through the bootloader code, and it seems that the bootloader checks the first bank address to be between 0x20000000 and 0x20040000, which fails because the initial SP is located near the end of SRAM which is at 0x20050000.for this chip.

could it be a bug in the bootloader code, or something im missing ? 

alternatively, how can i locate __init_sp in some lower address ?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on March 25, 2018 at 00:10

Just write a lower value in the first vector and load the SP with __init_sp in Reset_Handler

For GNU/GCC the stack is frequently defined in the .LD linker script.

...

; Vector Table Mapped to Address 0 at Reset

                AREA    RESET, DATA, READONLY

                EXPORT  __Vectors

                EXPORT  __Vectors_End

                EXPORT  __Vectors_Size

__Vectors       DCD     0x20002000               ; Top of Stack - Nominal RAM address, set to __initial_sp later

                DCD     Reset_Handler              ; Reset Handler

                DCD     NMI_Handler                ; NMI Handler

                DCD     HardFault_Handler          ; Hard Fault Handler

                DCD     MemManage_Handler          ; MPU Fault Handler

...

; Reset handler

Reset_Handler    PROC

                 EXPORT  Reset_Handler             [WEAK]

        IMPORT  SystemInit

        IMPORT  __main

                 LDR     SP,=__initial_sp ;; Set SP, for Keil also done in __main as I recall

                 LDR     R0, =SystemInit

                 BLX     R0

                 LDR     R0, =__main

                 BX      R0

                 ENDP
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2
Posted on March 25, 2018 at 00:10

Just write a lower value in the first vector and load the SP with __init_sp in Reset_Handler

For GNU/GCC the stack is frequently defined in the .LD linker script.

...

; Vector Table Mapped to Address 0 at Reset

                AREA    RESET, DATA, READONLY

                EXPORT  __Vectors

                EXPORT  __Vectors_End

                EXPORT  __Vectors_Size

__Vectors       DCD     0x20002000               ; Top of Stack - Nominal RAM address, set to __initial_sp later

                DCD     Reset_Handler              ; Reset Handler

                DCD     NMI_Handler                ; NMI Handler

                DCD     HardFault_Handler          ; Hard Fault Handler

                DCD     MemManage_Handler          ; MPU Fault Handler

...

; Reset handler

Reset_Handler    PROC

                 EXPORT  Reset_Handler             [WEAK]

        IMPORT  SystemInit

        IMPORT  __main

                 LDR     SP,=__initial_sp ;; Set SP, for Keil also done in __main as I recall

                 LDR     R0, =SystemInit

                 BLX     R0

                 LDR     R0, =__main

                 BX      R0

                 ENDP
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ron23
Associate
Posted on March 26, 2018 at 08:26

thanks, worked perfecly