cancel
Showing results for 
Search instead for 
Did you mean: 

Not able to boot up STM3241G-EVAL kit in my windows 10 laptop

Diwakar Ragupathy Raj
Associate II
Posted on March 21, 2018 at 14:16

Hi awesome people,

I am new to MCU programming and I am doing an image processing project in pattern recognition. I am using STM3241G-EVAL development kit. I am not able to boot up my kit on my laptop(Windows 10). I connected  the power cable and the usb cable but still its not booting up

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on March 21, 2018 at 16:33

Is there a jumper to select the power source?

Which USB? ST-LINK?

Is it running code that would support connectivity as a USB HS/FS device?

Does it power from 5V DC wall-wart supply?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on March 21, 2018 at 20:26

Ok, but what does '

not booting up

' mean to you?

Is this a new board, or has someone else used it already? Loading other examples will wipe the demo app.

Have you connected to the ST-LINK USB connector? CN21

Have you installed the drivers?

Have you build and downloaded any of the example applications?

Are you working with a local ST office or FAE?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on March 26, 2018 at 11:18

hey, 

thanks for your help. I tried changing the jumper and it worked. thanks a lot