STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! PWM/ADC HAL callback referall

Posted on July 08, 2018 at 12:14Hi,As we know peripherals can have callback functions such as the below one for the PWM:void HAL_TIM_PWM_PulseFinishedCallback(TIM_HandleTypeDef *htim) {}This is something like a general callback, But if we have sever...

STM32F745 RTC Runs fast

Posted on July 06, 2018 at 04:25I have a most interesting problem i am some what baffled to resolve. i am using an STM32F745IE CPU overall a very nice device. i have setup the CPU with a 25MHz primary crystal and a 32.768KHz crystal LSE solution. Th...

CAN slave and SRAM

Posted on July 08, 2018 at 15:52Hello, Thanks for all your wonderful support !i read the full CAN section in RM of STM32F446RE but could not able to understand how CAN2 differs from CAN1, why CAN2  called as slave ?its mentioned that , CAN2 cannot a...

RN by Senior
  • 586 Views
  • 0 replies
  • 0 kudos

STM32F373 DAC Issue

Posted on July 06, 2018 at 11:20The original post was too long to process during our migration. Please click on the attachment to read the original post.

Resolved! STM32F777 remapping/jumping to internal SRAM

Posted on July 07, 2018 at 14:54Hi,I was previously working on an stm32f429 MCU and successfully jumped to internal SRAM using:__HAL_SYSCFG_REMAPMEMORY_SRAM();I've ported my code to a new STM32F777 system and have realized the above function does no...

Update via UART without circuit jumper STM32F769

Posted on July 07, 2018 at 17:32Hello,I have a custom board with the MCU STM32F769. We integrate the board inside a machine. To update the software, the user has access only to RS232 and power ON/OFF switch.We use another controller (not from STM ) ...

An Ha by Associate II
  • 1053 Views
  • 1 replies
  • 0 kudos

HAL Timeout on UART Receive

Posted on November 06, 2017 at 23:55I'm setting up a UART channels to transmit and receive from a slave device.I have Transmit working as I can see the slave is doing what's asked from the command sent to it.On each command the slave reply's back wi...

Lalit B by Associate
  • 8365 Views
  • 4 replies
  • 0 kudos