User Activity

hello ,i want to have your advice in general:We use lcd 16x2 for our master device and 20x4( lcd needs 5 v power) for the end devices, in both we use keyad to make a PİN OUT RESET OF THE STM CHİP ,But for some device the lcd init happens very good fo...
hello i need to protect my code from reading or just protect the two first pages is enough because ill put my devices on market ? i cliked on execute only code option in keil flash options my code doesnt compile here is the error :..\Middlewares\Thi...
hello evry body i have a prblm i can read page 31 : 0x0800 7C00 and write of flashbut adress 127 (page127) adress 0x0801 FC00i have a prblm it doesnt allow reading or writingeven my stm is stm 32f103cb medium flash is 128kb , i dont understand why it...
HELLO ive created a project in cubemx v4.22. later i changed to new version i mean i downloaded the v 4.24.0 if i add iwdt then i get the project it doesnt compile , igot this error compiling system_stm32f1xx.c...linking...ROVER_LORA\ROVER_LORA.axf: ...
hello i try to read registers RCC_CSR with FlagStatusRCC_GetFlagStatus (uint8_t RCC_FLAG)but my project generated by cubemx doesnt recognize this function ,is there an option i didnt open on cube mx , or should i download a folder , because i couşdn ...
Kudos from