User Activity

Hi, i have a question about this. Normally we use F0 series and BOOT0 pin must be connected to GND via 10K Ohm. So, BOOT0 pin were apart. But now, BOOT0 pin and SWCLK pin is same. I created a new schematic and I connected BOOT0/SWCLK to GND via 10K ...
Posted on April 04, 2018 at 17:29Hi , I want to drive White Led 7 Segment Display. MCUs power supply is 3.3V (STM32F030C6T6), and white led voltage about 2.8V when the current is 20mA. So, light intensity is too low. Is there any way to increase int...