STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

custom multi touch USB_HID

Posted on July 09, 2018 at 15:32Hi all,I have few following doubts regarding board...please clarify them...1. is it possible to implement a multi touch USB HID descriptor?. Because, i have already implemented a single touch descriptor and tested on ...

How to update firmware while read protection is on?

Posted on July 09, 2018 at 10:55Hi all!I need suggestions to implement such mechanism like our smartphone(Update our phone without while working normally), i'm working on STM32L152 where i want to apply read protection to protect my code and when we...

Invitation to contribute a book chapter

Posted on July 09, 2018 at 10:45Dear All,I am Dr. Firouzi, an Editor of Springer. Currently we are editing a book on AI-driven IoT. One of the chapters is dedicated to Embedded System (Connected Devices): Page limit: 30-50 printed pages Beside the ...

Signal generation with dac and DMA problem

Posted on July 07, 2018 at 13:56So i am using stm32f469NI processor on discovery development board I already generated signals with processor , but that is not good since it doesn't allow for anything else to happen while the signal is being generat...

STM32F4 DMABMR

Posted on July 02, 2018 at 17:02HelloWe work on STM32F407 with the stack LwIP in order to do webserver.We have work in a first time and we have no problem to di webserver.Actually, we work on our board, with the same program and we have this problem...

STM32F072C8 MDIO MDC

Posted on July 08, 2018 at 05:05Hi  I would like to use the STM32F0 to run the MDIO\MDC in STM32F072C8, if can use the GPIO port to simultion the MDIO\MDC to PHY communication  or exmaples code can share with us .thanks

hsiao SW by Associate II
  • 2372 Views
  • 3 replies
  • 0 kudos

STM32F0 Discovery Board 5V Output Current Limit

Posted on July 08, 2018 at 10:31Hi all,I have a STM32F0 Discovery board and would like to use its 5V power pin (pin 1) to power external devices (LEDs).  The user manual UM1525 section 4.3 says that the power consumption must be lower than 100mA.  H...

jacky by Associate II
  • 3239 Views
  • 6 replies
  • 0 kudos

Resolved! CAN1 TX sending continuous messages

Posted on July 02, 2018 at 15:27Hello, I have 2 CAN nodes ( both are nucleo f446re boards) and both connected to separate transceivers . I am exploring CAN_Networking ( NORMAL MODE) given in the ST example .even if i Tx only one time, the Transmitte...

RN by Senior
  • 2465 Views
  • 3 replies
  • 0 kudos

Need suggestion for choosing microcontroller

Posted on July 08, 2018 at 15:06Hi Everyone,     I am thinking of designing wireless home automation product using IoT. Can anyone suggest which STM32 series is suitable for this application. I have knowledge in stm3f4 series. So i can easily learn ...

Yadav by Associate II
  • 1653 Views
  • 3 replies
  • 0 kudos