STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FreeRTOS V10

Posted on May 05, 2018 at 21:00The current FreeRTOS in the Cube Repo is V8.x.x.  Way down level.  Is there a reason why the repo has not been updated to V10?

tim3 interrupt not getting cleared

Posted on July 06, 2018 at 00:09I'm new to ST but have extensive experience with Eclipse and other ARM M cores..I created a simple 'blinky' program using STM32CubxMX and ST32M System Workbench on a STM32F769-DISC0 Discovery Board.The LED toggles onc...

STM32F4 timer 13 as master for timer 12

Posted on January 21, 2016 at 15:38 Can`t get the TIM12 to work in slave mode from TIM13 as master. /* TIM13 clock is 1us */ TIM13->CNT = 0; TIM13->PSC = ( TimerBusClock / 1000000U ) - 1U; TIM13->ARR = 0xFFFFU; TIM13->CCR1 = 0xFFFFU; ...

vlpasha by Associate II
  • 1677 Views
  • 6 replies
  • 0 kudos

HAL_Delay and UART problem.

Posted on July 06, 2018 at 14:09I have a problem with stm32f103, if insert in HAL_Delay(1000) in Serial Monitor i see incorrect results, but if i insert HAL_Delay(150) the results are correct. I do not understand why!This is the code:while (1) { HAL...

Power Management for STM32L4R9VI MCU

Posted on July 06, 2018 at 17:47We are currently working on a device for healthcare implementation and had chosen the STM32L4R9VI to meet our specific needs. However, we are stuck on finding a suitable battery-charge-management solution that is also...

STM32F103, HAL and timer(s)

Posted on July 06, 2018 at 12:24I created a new project (using CubeMx & Atollic TrueStudio) for STM32F103RB and tried to toggle a bit as quick as possible; I use TIMER2 and this function to initialize it:=======================/* TIM2 init function ...

RaduG by Associate II
  • 3542 Views
  • 7 replies
  • 0 kudos

OpenOCD support for STM32F469

Posted on July 06, 2018 at 16:24Has anyone ever tried to program STM32F469 discovery board using OpenOCD? I am receiving the following error. Any ideas to debug this or any leads on this is appreciated.embedded:startup.tcl:21: Error: Command/target:...

STM32F2 CAN no TX

Posted on July 06, 2018 at 16:30 Cube generated Keil project with CAN I have developing own SW for third-party HW, original SW working with CAN interface and CAN works good - so HW is OK. My startup initiate CAN with 500kb, and RX0 interrupt ...