STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4X6 RNG validation on 80MHz AHB

Hello,I require RNG's functionality for one of my commercial projects. Reading through the reference manual, it is mentioned that ST has validated RNG's performance for the following clock configurations:RNG clock: rng_clk 48MHz, rng_clk = 400kHzAHB ...

ADudk by Associate
  • 1139 Views
  • 1 replies
  • 0 kudos

Booting process of STM32 MCU

Dear All,I am new to ARM microcontrollers and about to start working on some application. Please explain me the complete boot process of STM32L476RG controller.Who has to write the boot code? If the answer is the programmer, what he has to write exac...

VDesa by Associate II
  • 2161 Views
  • 3 replies
  • 0 kudos

External EEPROM memory I2C 1Mbit with STM32F051

Hello,I am using an STM32F051 with an external EEPROM M24M01 memory of 1Mbit capacity (500 x 256bits)STMCubeMX has a proprietary library for use with external I2C EEPROM memory, but it is not suitable for the storage memory I am using.Would someone h...

How to synchronise two Nucleo-L152RE boards by SPI

Hello !​I​ am studing SPI. I was created two projects for my Nucleo boards, where one is master, and second is slave. I send data from master to slave and printing it to PuTTY.​A problem in synchronisation of two boards. Slave is receiving correct da...

Max75 by Associate II
  • 2922 Views
  • 3 replies
  • 0 kudos

STM32L4 I2C Multi Slave Issue

Good DayI am having an issue with I2C and hope someone can point me in the right direction.I have an I2C master and two I2C slaves on a bus. The master sends a message to the slave and then reads back the response from the slave, which works.If I add...

abotha by Associate III
  • 1901 Views
  • 1 replies
  • 0 kudos

STM32 I2C2 SDA improper data

I have already used I2C1 successfully on STM32F051. However, when I am trying to use the I2C2 on STM32F051R8T6, the problem is that the voltage level of the data received on SDA line seems to be chopped. Am I doing anything wrong with the initializat...

0690X0000060OtsQAE.jpg

Nucleo F767ZI - COM port over Jlink

Hi,I've upgraded my on board debugger from ST-link to J-link.Everything works as expected and I'm able to burn the flash and debug.However, when I used on board ST-link I was also able to connect to the board with PUTTY and direct my stdin/stdout to ...