cancel
Showing results for 
Search instead for 
Did you mean: 

Low Power for Interrupt Input Port

Peter Simpson
Associate II
Posted on April 27, 2018 at 04:31

Hi,

     Would anyone have advice about minimizing power consumption in an input port that generates an interrupt.

      I have a STM32L072 micro with reset switch on Port PB_8 to GND

      I am configuring it with 

      GpioInit( &Switch, SWITCH_PORT, PIN_INPUT, PIN_PUSH_PULL, GPIO_PULLUP, 1 );

      GpioSetInterrupt( &Switch, IRQ_FALLING_EDGE, IRQ_VERY_LOW_PRIORITY, &Switch_IRQ );

      to wake the micro when it is in low power sleep mode

      

      It appears that pull up does not work with the port after it is set as an interrupt so I have had to put a pull up resistor       on the port which I have changed from 10K to 100K without any change.

      If the port is configured as an interrupt  as above, in sleep mode it draws 300uA more than if I set to same port still       with the resistor and switch attached using

      GPIO_InitStruct.Pin = GPIO_PIN_8; 

      GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

      GPIO_InitStruct.Pull = GPIO_NOPULL;

      GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

      GPIO_InitStruct.Alternate = 0;

      HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

      Any advice on a port configuration that reduces the current would be appreciated

      Thank You

      Regards

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0