STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using PC_1 and PC_5 results in a faulty reading values, Why?

The question is regarding Nucleo-l476RG, I need to use 5 ADC, 12Bit. No matter what I do. I cannot see that these pins are connected to anything else. Why do I get a wrong reading on these GPIO? Please notice that my board is new .. the MCU is not da...

MJala.8 by Associate
  • 1347 Views
  • 2 replies
  • 0 kudos

How can I implement reset button functionality without actually pressing the Reset button on the board and using some special pins on the STM32F446RE Nucleo board to do so?

I need to implement the reset button functionality without pressing the reset button by using, maybe, a GPIO pin on the STM board by giving HIGH or LOW on a specific pin using a GPIO of the Raspberry Pi. How can I do that?

SSoni by Associate III
  • 3188 Views
  • 4 replies
  • 0 kudos

Running QSPI Samples on STM32F7 EVAL board

I'm trying to run the QSPI samples from the STMCube_FW_F7_V1.15.0 package on my STM32F7779I-EVAL board. They run with no error but there's point where the data read back is compared to the data written and they never match. I tried both the interrupt...

LRodr by Associate
  • 1722 Views
  • 4 replies
  • 0 kudos

6LowPAN on STM32 MCU's

Hi Guys,looking for advice on in relation to building a smart home automation system using STM32F407VET6 and 2.4Ghz transceiver modules (NRF24L01+).Are there existing libraries which will allow me to operate a 6LowPAN network using this hardware? I h...

JElph by Associate
  • 941 Views
  • 0 replies
  • 0 kudos

Flags for VBAT low-power mode?

I'm using a Nucleo F429ZI, and want to use the VBAT mode when the controller loses VDD. Are there any flags that are specifically set or reset when the controller enters or leaves VBAT mode? I read in a reference manual that a power-down reset is wha...

JChan.0 by Associate II
  • 1061 Views
  • 1 replies
  • 0 kudos

Bug in HAL_ADCEx_Calibration_Start

The function using ADC_CALIBRATION_TIMEOUT. This timeout is defines as:/* Fixed timeout value for ADC calibration. */ /* Values defined to be higher than worst cases: low clock frequency, */ /* maximum presca...

SIM900 question ?

Dear Members,I want to test my SIM900 module,Do I need something more from this code ?printf("TEST SIM900\r\n"); //usart_pstr("AT\r\n"); target =0; //UART1 selected printf("AT/r"); HAL_UART_Receive(&huart1, (uint8_t *)&RxModem, 8,100); ...