User Activity

Hi All, I'm working on a project wherein I required multiple UART. So, as suggested on my previous question, I've brought the NUCLEOF413ZH. Unfortunately, this NUCLEO has several issues. Currently, I'm using all the 10 UART, but some of them having "...
Hi All, I'm working on a project (Street Lamp), wherein we required some metering parameters. So, I've brought an EVALSTPM34 board for speeding up the development process. On the "STPM3x Evaluation software" I was able to read all the necessary param...
Hi All,Currently, I'm working on project wherein I need the maximum number of UARTs I can get. After doing some research, I came across the STM32F091VC controller which has the 8 UART (max number of UARTs ST can provide). Unfortunately, there is not ...
Hi all,I'm new with the PWM business, so, I'm referring the sample code (TIM_PWM_Input) provided in STM32F2XX stranded peripheral library . In the readme.txt file it is mentioned that we can measure minimum 915Hz frequency. But in my application, I w...
Hi All,     I'm developing a project, in which I've connected the MII port of STM32F207 with Marvel IC 88E6060 (Ethernet + fiber switch) MII port 5 but the firmware support (SPL for STM32F2XX) provides libraries for DP83848 PHY only.      Hence, if I...
Kudos from