STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DMA events from TIM1 - One Stream with 3 channels?

I've been reading the STM32F427 and I can't confirm my understanding - so I'd like to ask.I have data that I must push out a GPIO faster then should be serviced by an interrupt.My intent is to use TIM1 - set a period - then set 3 output compares havi...

Joe.H by Senior
  • 1477 Views
  • 4 replies
  • 0 kudos

Does a bare STM32 ARM Microcontroller come with a bootloader?

Hi guys, I am planning to buy a bare STM32 ARM Microcontroller and wanted to know wether it comes with a boot loader so that I can directly upload code using Keil u vision, STM32 Cube MX and a ST link V2. If there is no boot loader shipped with the u...

Sashvat by Associate II
  • 2548 Views
  • 3 replies
  • 0 kudos

How to organize the SPI transmit buffer?

Dear experts, can you please give a suggestion about how to proceed with the following problem?I am trying to display the information on the PCD8544-driven LCD (aka Nokia 5110) about the incoming UART messages.I am using STM32CubeMX to configure the ...

EOvch by Associate
  • 905 Views
  • 0 replies
  • 0 kudos

Resolved! SPI RX buffer shifted

Posted on February 23, 2018 at 18:10Dear All,I use SPI as a master with 2 lines full duplex with DMA on STM32F303RE with 8-bit data size.Frames are made of variable number of Bytes. Normally SPI clocks out 3 Bytes of command on MOSI line + 4 Bytes o...

sirpak by Associate II
  • 7568 Views
  • 11 replies
  • 0 kudos

ADCs in Dual (Multi) Mode in F446

Hello AllI have configured ADC1 and ADC2, each with CONT=1 and L = 0, to convert two respective analog inputs on a software start, and the scheme works fine. However, when in the CCR I set the MULTI bits to 0b00110 (or to anything else for that matte...

Amir1 by Associate II
  • 670 Views
  • 0 replies
  • 0 kudos

STM32L100 RTC

Hello!In my design, I want to use the STM32L100 series microcontroller. How can I get a clock frequency RTC of 1 Hz if I use a highly stable external oscillator with a frequency of 30 MHz to clock the microcontroller.PREDIV_A can be 1,2,3, ..., or 12...

EChum by Associate
  • 929 Views
  • 2 replies
  • 0 kudos

Dead time insertion

Hello,In my application I need insert dead time only for upper transistor in bridge. Does anybody know how to insert dead time without using CubeMX because?Can you provide me an example of code and literature?Thanks a lot,

DBake.18 by Associate II
  • 794 Views
  • 0 replies
  • 0 kudos