STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STMPE811 touch controller Interfacing with STM32F746BGT6

We are developing the TouchGFX project in  STM32F746BGT6 and using resistive TouchscreenWe have created the project using ST CUBEMX for discovery board .the same project code has been used for our customized PCB.For this we need to interface the STMP...

STM-User by Associate II
  • 947 Views
  • 0 replies
  • 0 kudos

Hard reset Interrupt issue in STM32F103RB

I am testing EXTI interrupts on STM32F103 board. The device works properly when soft reset is given. Interrupts are triggered properly. But when I give hard rest to the device(Like power off & power on) , it fails to initialize STM32. Maybe it gets a...

sne_123 by Associate III
  • 900 Views
  • 0 replies
  • 0 kudos

Resolved! How do the GPIOs actually work?

That question started bothering me when I was struggling with TLE493D that started interrupting using the i2c clock line.It looked like the i2c in the F429 was gone bananas and keeping the i2c stuck (busy).I was thinking of feeding the i2c the clock ...

STM32F103RCT6 I2C SLAVE transmitter CAN NOT GENERATE ACK

Currently I try use STM32F103RCT to implement I2C slave to communicate with master. When master sent address with write bit , there is no any problem and all data can be transmitted to slave through I2C, but when master try to read, it seems big prob...

Liu0155 by Associate II
  • 1046 Views
  • 1 replies
  • 0 kudos

Using STM32F105RBT6 with a 4-pin oscillator?

I'm using a STM32F105RBT6 in LQFP64 package in a project. The datasheet suggests using a crystal or resonator. I want to use a 4-pin oscillator that has a single output pin. Is this possible and if so where do I connect it?Thanks.

JBosi by Associate
  • 2432 Views
  • 4 replies
  • 0 kudos

Resolved! Error in the reference manual?

Hello,I would like to signal a possible error on the reference manual of the STM32L496 (RM0351 Rev 6)At pag 348, section 11.4.5, Table 45 the first line (source port 8bit, destination port 8bit) indicates that the Number of data items to transfer is ...

ADC DMA not work

HelloWe ran the ADC DMA on the HAL example source. However, I tried to write the source in CUBEMX, When executed, the DMA interrupt is executed once and is not executed again.Please let me know if I missed anything

HG LEE by Associate II
  • 1231 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.