User Activity

Hello everybody,i wanted to send data from realterm serial to the stm32F767ZI but it dose not work. i cant see any message on my terminal. The same code is working good with STMF446re. The UART2 with STM32F4446re is connected to the USB Port. but wit...
Hallo everybody,i would like to generate analog signal (0-5 V) via DAC but the problem is the maximam voltage is 3.3 V . ist it possible to change some configuration to generate an analog signal with maximam voltage from 5 V? thanks #DAC​ #[Analog an...
Hello everybody,I want to measure   the duty Cycle of a PWM Signal in Simulink. . I have managed it to  generate a  PWM signal with Simulink and STM32 MAT-Target. The problem is  now when build  a simple model to generate the code, the lines between ...
Hallo,2 STM32 μc (NucleoF767ZI and Nucleo F446RE) should communicate via SPI. The first µc is programmed with Simulink using the Nucleo Support Package. As it stands, the μc with the Support Package can only work as a master. Now I just want to send ...
Hello everybody,I wanted to measure the duty cycle (tone) of a PWM signal with input capture mode. Unfortunately, it works only almost up to 65% of the duty cycle(Ton). otherwise will the T_off measured instead of Ton. does anyone have an idea what c...
Kudos from