User Activity

Hello,According to data sheet on STuW81300 the ST1.PLL_SEL must be 1 and Nint, Frac must be calculated based on formula on page 25, when VCO frequency if higher than 6GHz. In this case the sub-harmonic at half frequency appears. How could be this sub...
Hello,When the ST1.PLL_SEL is set to 1 for VCO Frequency > 6 GHz, the sub-harmonic at half frequency appears. How could it be eliminated? Thanks,Alex
Hello, It looks like the synthesizer STuW81300 has RF power degradation across frequency (power is +4dBm at 4GHz and -4dBm at 7.5 GHz). We can't reach declared in data sheet +8dBm at RF1_OUT. How we can control RF power for STu81300 e.g. similarly as...
It is not clear from documentation: What is active level for input signals HW_PD(pin 4), PD_RF1 and PD_RF2 (pins 5 and 6) ?Thanks,Alex
Hello,I've faced some problems with setting up and sending data for STM32L496 Serial Audio Interface (I2S) using HAL functions from the PACK. Could you recommend some software examples or a sequence of actions? Thanks,Alex