STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H753 schematic and footprint

Hi, where can I find schematic and footprint for STM32H753 (or STM32H7 xx family) for Altium? In the STM32H7 and STM32H753 page I cant find nothing.Best regardsGMG

GMG by Associate III
  • 3401 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H7 triggering ADC with TIM6 TRGO

The ADC (ADC3 if that's relevant) provides for triggering by way of the TIM6 TRGO event. I have the ADC configured to convert with "ExternalTrigConv" pointing to ADC_EXTERNAL_TRIG_T6_TRGO, and the update event's rising edge. In no case am I able to g...

n2wx by Senior
  • 8742 Views
  • 25 replies
  • 1 kudos

STM32F427 SDIO Block Write with DMA not responding properly

I don't use libraries.My SD card interface is set up with an SDIO clock of 16.67 mhz using the 4-bit interface.My block write (SD command 24) works properly if I poll the data into the FIFO. The problem with that is the timing to push data into the F...

0690X000008wPbiQAE.png 0690X000008wPbsQAE.png 0690X000008wPbxQAE.png
Joe.H by Senior
  • 5365 Views
  • 5 replies
  • 0 kudos

Audio Driver Issue on STM32F769I-Discovery board

I am using STM32F769I-Discovery board with STM32Cube_FW_F7_V1.16.0. I have the following issues on the audio driver functionality: I am trying to record the audio with sample audio application provided as part of this package. The driver by default ...

RSani.1 by Associate
  • 1108 Views
  • 0 replies
  • 0 kudos

STM32F746 SPI DMA Transmit and Receive issue.

Hello, I generated project with STM32CubeMX. I configured it in SPI slave with DMA Seems like memory increment mode in not working. When I check register DMA_SxCR MINC is off. But when I checked hdma_spi2_rx.Init.MemInc , its has correct DMA_MINC_E...

Strange behaviours of SPI bootloader on STM32F412

I'm developing a SPI bootloader, using the integrated function of STM32F412, and I found two strange behaviours:I must issue two times the reset of MCU with Boot0 high, because after the first reset the MCU seems to be in bootloader mode but doesn't ...

Guidoted by Associate III
  • 2798 Views
  • 6 replies
  • 0 kudos

White screen with STM32F767 BITx microprocessor

Hi, I am working with a customized board which has STM32F767 BITx microprocessor. I made a simple application with TouchGFX 4.13.0 integred with STM32CubeIDE 1.2.0. The program builds and debugs correctly, but nothing appears on the screen, it is jus...

DCost.1 by Associate II
  • 711 Views
  • 0 replies
  • 0 kudos