2019-10-11 3:34 PM
I have a board with stm32f415 that use the bxcan that continuosly (8 packet every 10 seconds ) trasmit to another receiver board that use Microchip MSC2515 as CAN controller.
Some of the packet that i sent from STM32F415 contains all zeros bits. I have used a CAN Analyzer that detect many RX_Error passive. I have try to change the content of my packet replacing the 0x00 byte to 0xAA byte and magically the RX_error counter of the CAN Analyzer does not increase.
There may be a difference of bit stuffing implementation between Microchip CAN controller and ST can bxcan Controller ?
Or there is a configuration bit to set HW bit stuffing?
thanks
Dario
2019-10-14 4:14 AM
Missing termination? Bad wiring? Electromagnetic noise?
2019-10-14 4:52 AM
-n°2 120R are place at the ends of the bus
-I have used CAT6 cable , but the distance is max 15 meters and baud rate is only 50Kbps
-Electromagnetic noise? I believe not, because the same behavior is done both at home and in the factory
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.