2019-10-13 11:05 PM
"The operating temperature has an impact on the accuracy of the RC oscillators. At 25 °C, the HSI16 oscillator has an accuracy of ±1% typically, the MSI oscillator has an accuracy of ± 0.5% and the HSI48 oscillator has an accuracy of ±4%."
It is described on page 1 of AN4631 How to calibrate an STM32L0xx internal RC oscillator.
One of the Ceramic Resonator(HSE ) has Frequency Shift by Temperature +/-0.20% max.
Frequency Tolerance +/-0.50% max.
Operating Temperature Range - ℃ 20 to ℃
Just want to know what is the frequency shift by temperature for STM32L0xx MSI(Multi-Speed Internal)?
Thanks and Best regards,
E-John
Solved! Go to Solution.
2019-10-14 12:21 AM
This sort of thing would normally be in the data sheet for your stm32 (unless it is so new this has not been characterised)
For example stm32l031 data sheet Rev 4* has in the "Electrical Characteristics" "Operating Conditions" "Internal Clock Source Characteristics" a table on "MSI Oscillator Characteristics" - Table 43 on pages 72-73
It says the MSI might vary by 3% over temperature, and 2.5%/V over supply-voltage.
Don't rely on these variations to be linear. Chip designers use a lot of "tricks" to eliminate variations as best they can (for example current sources that are "PTAT" (proportional to absolute temperature).
Hope this helps,
Danish
*Possibly not the most recent but that's the one I downloaded when looking at this chip to see if it was the right one for a particular project, so the table or page numbers might have changed
2019-10-14 12:21 AM
This sort of thing would normally be in the data sheet for your stm32 (unless it is so new this has not been characterised)
For example stm32l031 data sheet Rev 4* has in the "Electrical Characteristics" "Operating Conditions" "Internal Clock Source Characteristics" a table on "MSI Oscillator Characteristics" - Table 43 on pages 72-73
It says the MSI might vary by 3% over temperature, and 2.5%/V over supply-voltage.
Don't rely on these variations to be linear. Chip designers use a lot of "tricks" to eliminate variations as best they can (for example current sources that are "PTAT" (proportional to absolute temperature).
Hope this helps,
Danish
*Possibly not the most recent but that's the one I downloaded when looking at this chip to see if it was the right one for a particular project, so the table or page numbers might have changed
2019-10-14 12:47 AM
Never heard of a "Multi-Speed Internal" oscillator, it seems new with this part - or family.
As you cited the tolerances of other oscillators, I suppose this specific one is missing from the datasheet.
Mistakes happen, so I would inquire ST directly. An perhaps ask for an updated datasheet.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.