STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 ADC overrun errors

Hi, I have a problem configuring ADC1 on an STM32F429 to do a regular scan of a sequence of 4 channels without using DMA. The fourth channel is the internal temperature sensor. The third channel to be scanned always gives an overrun error (ADC_SR.OVR...

ScottT by Associate
  • 2000 Views
  • 2 replies
  • 0 kudos

RAM retention between resets.

Hello,How do I retain a RAM section from bearing filled with '0' between resets.Suppose I have a pointer to 256 bytes buffer that I'd like to preserve between resets (as long as the power was not disconnected), could you please guide me, step by ste...

EMich by Associate II
  • 2750 Views
  • 2 replies
  • 0 kudos

ADC reading three channels

Hi,I would like to create an ADC driver for reading three channels, but I don't understand how I can read the single risult. I wrote a driver that read one channel (As you can see in attached file), What are the istructions for adding others channels...

LBern.1 by Associate
  • 1061 Views
  • 0 replies
  • 0 kudos

stm32F407, stm32F072 and CAN bus

hello, i am trying to connect a stm32F407 and stm32F072 via CAN bus. but i cnt manage to get it done. i successfully connected two F407 via CAN bus and i used the same code for both of the boards . both of them transmitt the data perfectally but none...

SGUIG.1 by Associate II
  • 1252 Views
  • 0 replies
  • 0 kudos

N-pulse waveform generation application example - part2 (AN4776)

Hi .I have problem with this back to back timer configuration . (in AN4776)What I get :1- Timer 1 is making PWM ( i just need a regular pwm but this examle is a complementary one )2-Timer 1 will send a trigger to timer2( which is it's controller acut...

0693W000001pLJoQAM.png
M N by Associate II
  • 2298 Views
  • 6 replies
  • 0 kudos