STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! PWM mode and ARPE bit | Confirmations

Hi everyone,I am dealing with the configuration of a PWM in center-aligned mode in the context of the stm32H755 MCU. Such PWM is managed using TIM1 as "driver". The application requires to change every 100 us (TIM1 period) the ARR register to make it...

Zzaaack_0-1748528362740.png
Zzaaack by Associate III
  • 1292 Views
  • 3 replies
  • 1 kudos

Dead Time In General Purpose Timer

I have a doubt about can a general purpose timer generate dead time like advanced timer without changing the duty and frequency is this is possible i tried with center aligned mode but it changes the duty is there is any possiblities??

LPTIM with RepetitionCounter dosnt work

Hello,I need counter which should wakeup system from stop2 mode at every sequential time.So currently use below setting and it works fine and wakeup at every ~4.16 minutes. But I want it should wakeup at max time of 30minutes (not fixed but looking f...

Debugging an application run from external flash memory

Hi,Is there any way to debug an application launched from external flash memory? I use J-Link and IAR, the application is loaded into flash but I am not able to start debugging. I assume that in order for the microcontroller to even start executing c...

Artur5 by Associate III
  • 934 Views
  • 1 replies
  • 0 kudos

Resolved! Flash structure confusing page number

HiiI am using stm32g0b0cet6, while writing bootloader, i am confused with the page number and the total storage.Its total storage is 512 kb, According to the reference manual, The Main memory is shown like belowQuestion1: If each page is 2kb & total ...

skuma8_0-1748584125478.png
skuma.8 by Associate III
  • 822 Views
  • 1 replies
  • 0 kudos

Stm32h743ii 2 i2c independant bus

 Dear all; I have a *** question but it dont work can we have quantity 2 different i2c bus 1 is reconized but not the second bus  /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_LTDC_Init(); MX_QUADSPI_Init(); MX_FMC_Init(); ...

KNaim.1 by Associate III
  • 2101 Views
  • 6 replies
  • 3 kudos