User Activity

Hello,I stumbled across a probably already wellknown problem:unable-to-use-quadspi-status-flag-polling-mode-with-instruction Now I'd like to know if there are any news, somebody wrote that the issue is observed by ST.Second I'd like to know if newer ...
Hello,I configured QSPI and MDMA in CubeMx and generated the initialization code. I merged the flash demo code (QSPI_ReadWriteDual_DMA), available for the H743 evaluation board, into my project.Regarding the QSPI waveform I'm puzzled whats going on d...
Hello,I have a NOR SPI flash connected to single SPI interface of a H75x MCU and want to use the highest possible SPI frequency for data read. The core clock is 400MHz, so I can chose between 50 and 100MHz.According to the data sheets the "Clock low ...
Hello,I'm using the HAL_SPI_TransmitReceive() to communicate to a NOR flash via single SPI in polling mode using HW CS. I'm on H753 Rev.V silicon using the latest HAL library.I checked out the SS output management in master mode (SSOM=1) but made str...
Hi,I want to generate code and project files for MDK-ARM and STM32CubeIDE.For this I created a new directory and copied the .ioc file into it and opened it it with CubeMx (latest version 6.13).In the projectmanager/project the following directory str...
Kudos from