STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I have a B-L475E-IOT01A. I am having issues reading value into the ADC. My values change but only slightly. I am testing it a POT from 0 to 3.3V as verfied by an volt meter.

 I seem to have things configured correctly. This is the bulk of my code:  while (1)  {    /* USER CODE END WHILE */    /* USER CODE BEGIN 3 */    HAL_ADC_Start(&hadc1);    while (HAL_ADC_PollForConversion(&hadc1, HAL_MAX_DELAY) != HAL_OK);        ad...

ALivi.1 by Associate
  • 765 Views
  • 0 replies
  • 0 kudos

Complementary of square signal

Hi All;I used the following instruction for STM32F429I, but there is error.Could one help me please. void EXTI0_IRQHandler(void){ if (EXTI_GetITStatus(EXTI_Line0) != RESET) // Here the ERROR <--------------------{ /* USER CODE BEGIN EXTI0_IRQn 0 */ i...

AAbed.1 by Associate III
  • 1150 Views
  • 1 replies
  • 0 kudos

Updated time of RTC is not being read

I am running RTC for stm32h753. If I read the time of RTC, I do not get updated value as shown in below example. I am using LSE 32.768Khz. As it can be seen that 00:08:10  is being read repeatedly and then 00:08:15. if I compare overall time, it is ...

Resolved! Weird (for me) problem(s) with ADC and DMA on STM32F3348

First, I have done this before successfully on the STM32F446re with all 3 ADCs and DMAs but I need some guidance or ideas... STM32F3348 Disco OR my target PCB with same processor. ADC1 (and maybe ADC2) using DMA to convert 7 channels on ADC1 and 4...

how to use ADC in discontinuous mode without HAL?

I am trying to use the ADC without using HAL (except for in the setup) on a STM32F031K6, using cubeIDE. Im using the ADC in discontinuous mode - as far as I can tell, the sequence of events should be  - ADC is setup, then enabled with ADEN - ADC star...

deep_rune by Associate III
  • 1859 Views
  • 0 replies
  • 0 kudos

Resolved! Correct sequence to reconfiguring CAN FD settings

Hi,I've been trying to get my CAN FD configuration going, but I'm running into issue when I need to reconfigure the timing parameters for different bandwidth.My original code, generated partly by CubeMX looks like this: hfdcan1.Instance = FDCAN1; ...

TOlli by Senior
  • 1655 Views
  • 1 replies
  • 0 kudos