cancel
Showing results for 
Search instead for 
Did you mean: 

CAN2 peripheral configuration

NSood.1
Associate

I have this code attached which is configured to run both CAN1 and CAN2 peripherals however the TX functionality which is what I was trying to use is working on CAN1 but not on CAN2 (trying to send a packet using ADDmessage TX routine), I double checked with another sniffer hardware and CAN1 works.

However, I'm configuring the CAN2 with exactly the same parameters as that of the CAN1, is it right or does CAN 2 have to have different settings!?

System is STM32F429 discovery board with SN65HVD230 transceiver.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0