cancel
Showing results for 
Search instead for 
Did you mean: 

Can I configure Octo-SPI to QSPI (4: 7) and then communicate with the NAND-FLASH of the QSPI interface?

WDong.1
Associate

Octo-SPI can be configured as QSPI (0: 3) and QSPI (4: 7). Can these two interfaces be connected to QSPI-FLASH interface? For the convenience of PCB, I want to use QSPI (4: 7).

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Andreas Bolsch
Lead II

The OctoSPI does support dual-quad mode as well, so yes, it's possible to connect two flash chips in QPI mode, one of them using IO7-IO4 the other one IO3-IO0. If you have only one, set DQM to zero and select via FSEL whether you want to user the "upper half" or the "lower half". This works exactly in the same way as for the QSPI interfaces.

See e.g. Fig. 136 in RM0455 for H7A/B and the description of OCTOSPI_CR, bit 7, FSEL.