Octo-SPI can be configured as QSPI (0: 3) and QSPI (4: 7). Can these two interfaces be connected to QSPI-FLASH interface? For the convenience of PCB, I want to use QSPI (4: 7).
When I choose STM32H750VB, the number of RGB integers is not enough (sufficient to use 565 mode), and it is scattered. In order to facilitate the connection, can I mess the order of each color number?