STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is it possible to stop ADC-DMA transfers when debugging?

I have an ADC1 setup in continuous mode and DMA1 in circular mode setup to transfer adc data to a circular buffer in memory. The data is processed directly from the circular buffer and the buffer is big enough that the processing is done before the b...

Fibo by Associate II
  • 2887 Views
  • 2 replies
  • 0 kudos

Will dividing down an external clock add jitter?

I read in the general timer manual for the STM32 (AN4013) that the external clock inputs (ETR, TI1, and TI2), which can be used for timer inputs, are synchronized internally with the APBx clock.I just want to make sure I am understanding this correct...

Use the CAN with the F469-Discovery

It's possible to use the CAN with the STM32F469I-Discovery?I have saw that the CAN1 pins are used for the touchscreen (I2C), so i can't use it. I can use the CAN2, but it's a slave on the STM32F469.  I have read that if I want to use the CAN as a sla...

Luca1 by Senior
  • 1695 Views
  • 2 replies
  • 0 kudos

Resolved! I need to be able to count pulses that are incoming on a GPIO. What is the best way to do this? Timers?

I have an application where I need to count the total number of pulses coming in from a fuel flow sensor. I then take the total number of pulses to display a readout of the total amount of fuel that has flowed through the sensor since the counter beg...

NChal.1 by Associate II
  • 4902 Views
  • 5 replies
  • 0 kudos

which (small but powerfull) board for dsp ?

Hello,I want to DSP an audio signal to create guitar effect(s), and someone pointed me the Nucleo boards, - are they the right choice for DSP ?- if yes, which have a narrow/small footprint board (similar to teensy 3.6 or RPI zero)the product selector...

PF.1 by Associate II
  • 14953 Views
  • 35 replies
  • 0 kudos

STM32 Clear Serial Monitor Screen

Hello, I am writing an application for STM32H7. I need to clear serial terminal the screen before showing the new lines on the terminal. Can anyone please help? Thank you in advance. Vouria

VYoun by Associate III
  • 3581 Views
  • 1 replies
  • 0 kudos