STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Peripheral examples for stmf32

Deat ST Hello,This my first question to you in this forum.Does ST has peripheral examples using HAL library or standard lib for STM32f4?I am installing the packs from the pack installer from Keil.Could I adapt examples for my STM32 if ST provide a g...

Check FlashErased or Readout InternalFlash ECC on STM32H7

I'm working on the STM32H7 series, and in my scenario the data to be written might be the erased-state byte (0xFF) all over the flashword. In this case I'm unsure whether or not the ECC may change.What is the idiomatic way of checking if the bytes ha...

FDane by Associate II
  • 627 Views
  • 0 replies
  • 0 kudos

STM32 TSC is not working

I am using Group1 for shield and Group 2 and Group 3 for touch keys but the after generating the code from cube mx ​there is a problem in firmware because group 3 touch is not working and touch is detecting from the shield. Please give me any solutio...

Smalik by Associate II
  • 889 Views
  • 1 replies
  • 0 kudos

Linux driver for TPM ST33TPHF2ESPI

HelloI'm following the instruction of https://www.st.com/resource/en/data_brief/stpm4raspi.pdf to setup the tpm driver on my embedded linux using ST33TPHF2ESPI tpm module. But unable get /dev/tpm0 and /dev/tpmrm0 present due to driver read spi failed...

0693W000001rsgzQAA.png 0693W000001rsh4QAA.png
GChen.3 by Associate
  • 1996 Views
  • 1 replies
  • 1 kudos

Implement PWM dithering 1 bit

Hi I am working on stm32f070. The STM32F0 system clock = 48MHz,I need to set the PWM frequency on 23437Hz.Therefore, PWM resolution = 48MHz / 23437Hz = 2048 (11bit)​How to use PWM dithering technique to reach 12-bit resolution on PWM frequency 23.4KH...

sam_cheng by Associate III
  • 3071 Views
  • 5 replies
  • 0 kudos

STM32F7 FMC Nor Flash Problem

Hello everyone,I have designed a board with STM32F750N8, 22 Bit Parallel Nor Flash, 13 Bit SDRAM, QSPI Nor Flash.Now i am trying to read, write data, read device id from fmc nor flash (other memories not enabled). But when i try to read device id, ge...

want to zip and unzip assets in stm32f4 MCU

Hi All,I am using STM32F429ZIT6 MCU. And we were planning to zip the assets and unzip them inside MCU. Please can anyone suggest the best starting point for good libraries which can do this.Thanks,krishna

Kpodu.1 by Associate II
  • 5405 Views
  • 4 replies
  • 0 kudos

ADC Error to HIGH.

Hey Everyone;I`m working with the STM32L031K6T6 in a project that I require 2 ADC channels. The ADC look to be working with a huge measurement error:Project description:Signal Type: Sinusoidal ( 1Vpp) with offset of 1.492 ( Offset provide by independ...

0693W000001t4AZQAY.png 0693W000001t4BvQAI.png 0693W000001t4CAQAY.png 0693W000001t4D3QAI.jpg
CMart.3 by Associate II
  • 2112 Views
  • 3 replies
  • 0 kudos