STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L496VGT6 - Does anyone know for a fact that receive works on USART3? Please no "assumptions" -- I already did that.

Transmit works to PC via FTDI cable.Receive works from PC to PC (TXRX looped) So FTDI transmit working.Receive generates no interrupt.Receive sets no status.Receive data register remains zero.As GPIO, receive pin sees signal.It is as if the alternat...

How to "printf" on STM32F746-DISCO ?

I followed the step on the following video without the configuration of SD card. (I don't need it)https://www.youtube.com/watch?v=4f-leBIJkRY​Whenever transmitting 10 characters, the program broke bown on 11-th character as below: printf("12345678901...

Ellaine by Associate II
  • 2766 Views
  • 5 replies
  • 0 kudos
Axcvn.1 by Associate II
  • 4643 Views
  • 8 replies
  • 0 kudos

STM32H747 Discovery - DMA not starting

Hi, I tried to translate my 32F746 Discovery Audio program (SAI with DMA DB Mode) to the STM32H747 Discovery Board (using the M7). SAI and DMA are correct configured. I am not able to start DMA1 Stream 0 or to set the S0CR EN Bit manually. SAI is st...

DBrow by Associate II
  • 1876 Views
  • 3 replies
  • 0 kudos

QUAD-SPI too busy!

Hi guys,i am using the QuadSPI periphery to interface with a FPGA. I am in need of raw throughput with alternating write and read cycles of some number of bytes. I am just concept-prooving right now.Since QUADSPI->CCR is not allowed to be modified wh...

_legacyfs_online_stmicro_images_0693W000001qTAI.png
Albi G. by Senior
  • 9070 Views
  • 21 replies
  • 0 kudos