User Activity

I'm trying to get USBX Device MSC to work in Standalone mode (without RTOS).  I loosely followed @B.Montanari 's example in https://community.st.com/t5/stm32-mcus/how-to-implement-usbx-in-standalone-mode/ta-p/614435, and also referred to a CubeMX exa...
Over the last couple of years it appears that ST pivoted towards Azure RTOS / ThreadX as the default RTOS for newer STM32s like the STM32U5.  This seems in part to be because of the more cohesive set of packages like USBX, FileX, etc. on top of the b...
I'm hoping this is a simple question. In the reference manual (RM0394 section 39.4.5), the tolerance of the LPUART receiver is specified in Table 204. For example, with BRR = 1024 and 9 bits/1 stop bit, the tolerance is given as 2.33%.I've been ass...
Hi,I am trying to get some clarification on the accuracy of the STM32L4's HSI16. AN4736 mentions that the HSI16 will leave ST's factory calibrated to [-0.75%, 0.5%] at 30 C. DS11453 section 6.3.8 shows that the drift over 0 to 85 C will be -1% to 1...
Kudos from