In the last 2 days I can't get any results using search engine on the website. For instance, when I type in any STM32H743II code there is only a message like in the picture below. The same situation is for any acronyms or Doc Ids. Is it only a proble...
Dear CubeMX Team,Is there a chance to add DMA2D to the Peripheral list in CubeMX filters?Today, I can only find GFXMMU, but no DMA2D. Providing this option would save time for some of us looking for MCU with basic GFX support.
Is there any plan to provide Unique Device ID registers, together with second calibration point for Temperature Sensor in STM32G030xx?Initially, I expected these data being missing in stm32g030xx.h and DS by simple mistake. I really miss these 2 feat...
Dear ST Team, could you please update this section with correct information?There is incorrect text description or figure in RM0454 Rev 2 in section 14.10 (VBAT).Text: "...converted digital value is half the VBATvoltage."Figure: VBAT/3.
It's not only about the USBX Device Audio class, but it's a general remark. When I import the existing project into CubeIDE workspace, I only get the minimum set of files. The most important source files are not available or they are replaced with te...
Could you please consider turning off the default setting for the system clock resolver in CubeMX 6.3?It's very, very annoing when I have to fight with the tool, to get the settings I want. For instance, when I try to select the multiplier from the l...
Dear STMicroelectronics,Hereby, I would like to confirm that my system also blocked the application due to security reason.'Windows SmartScreen Filter disabled unrecognized application. Running this application can harm the system.Origin: UnknownAppl...
Thank you all for providing a basic questions. Sometimes I sit to close to the screen to see the obvious errors. Unique ID registers are available at locations starting from 0x1FFF7590. I found the error in my address definitions taken from STM32L03...