cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L4 LPUART receiver tolerance

PRuss
Associate II

I'm hoping this is a simple question. In the reference manual (RM0394 section 39.4.5), the tolerance of the LPUART receiver is specified in Table 204. For example, with BRR = 1024 and 9 bits/1 stop bit, the tolerance is given as 2.33%.

I've been assuming this means that all of the sources of baud rate error need to stack up so that the total is no more than +/- 2.33%. Is this understanding correct, as opposed to 2.33% total (+/- 1.165%)?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

Yes, it means ±2.33%.

If you feel a post has answered your question, please click "Accept as Solution".