STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H743VGT6 and STM32H723VGT6 - XIP Support on QSPI?

We are currently using the STM32H723VGT6 MCU (1MB Flash) in our application.We would like to clarify whether this MCU supports execute-in-place (XIP) from Quad-SPI flash or if Octal-SPI is required for XIP functionality.In the future, if our applicat...

LP257_0-1748509800393.png
LP257 by Associate II
  • 1382 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H743XGH6 USB VBUS

I want to use port PA9 of STM32H743XGH6 as “FS_VBUS”. In this case, which number should I put in the target register for the alternate function? I understand that if I use CubeMX, it will set it automatically.

NiM by Associate III
  • 3529 Views
  • 8 replies
  • 11 kudos

Resolved! STM32H7x3 USB Microphone Driver

Hi,I want to configure my device as a USB Microphone. However the cubemx generates code for USB speaker and the device is detected as STM32 Audio Class Speaker. Can anybody suggest a solution or Cube Example for USB Audio class with Microphone  codes...

Resolved! BOR in STM32U083

Hello,I found some discrepancy in BOR configuration for STM32U083CCT6 processor between reference manual [1] and HAL implementation [2]. It concerns BOR_LEV[0:2] bits (bits 10:8) in FLASH_OPTR register. The RM [1] talks of four levels (000: 1.7 V, 00...

KSzcz.2 by Associate II
  • 1604 Views
  • 3 replies
  • 1 kudos

T bit confusion

Hi,1.As it is mentioned in CM4 user guide and also explained in tutorial, 0th bit of PC is directly loaded to T bit.And CM4 supports only thumb state ISA.To execute/decode instructions in Thumb state 0th bit of PC should be 1 which means PC should al...

Screenshot 2025-05-23 141117.png Screenshot 2025-05-23 141211.png

STM32H7A3xI/G ADC frequency limitation

I am not sure I properly understand the STM32H7A3xI/G ADC frequency limitationIn the DEV13195 - Rev8 - Datasheet, section 6.3.21 16-bit ADC characteristics, table 93 ADC characteristics, page 143It says the fADC max frequency is 50 MHz with boost mod...

Neiluj by Associate
  • 1941 Views
  • 3 replies
  • 1 kudos