STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SIL 2 micrcontroller requirement

Hi, We are working on railway projects where we are looking for SIL 2 microcontroller. As per our analysis we found out that we need to integrate the X-CUBE-STL package to make it to SIL 2compliance. And we have found out that it should have supporte...

rajath by Associate II
  • 4066 Views
  • 13 replies
  • 3 kudos

Open web server data for B-U585I-IOT02A

Hello,I updated my development kit with the example IOT_HTTP_WebServer from the example selector in STM32 IDE. Then I needed to upgrade the firmware on wifi module, which seemed to work. I think I can connect to wifi, but I cannot open a webpage when...

GTanova by Associate III
  • 1039 Views
  • 1 replies
  • 0 kudos

Resolved! STM32U5G9ZJT6Q: three displays (two SPI and one 24 RGB)

Hi, good morning to all. I'm in the process to design an application based on STM32U5G9ZJT6Q. My first question, please, is: is it possible to have this STM32 drive three different displays, and possibly have TouchGFX manage the whole three ?In my ca...

Matbonny by Associate III
  • 1823 Views
  • 5 replies
  • 0 kudos

STM32H735-DK LWIP pbuf assertion issues

I've been struggling with a variety of issues with FreeRTOS/LWIP/DHCP/MDNS, before I've even got to implement my application code (which will be a UDP app). I've read all of the documents that have been linked in the forums, I've gone through the off...

i2pi by Associate II
  • 1299 Views
  • 2 replies
  • 0 kudos

STM32G474, USB, and CRS not working in concert

Greetings,We have implemented a USB peripheral on the STM32G474RE discovery board using code that runs properly on the STM32WB and STM32F0 parts.  On the G474, the USB setup completes, but the USB bus quickly suspends after the completion of the conf...

STM32H563ZIT6 SPI 16 bit with GPDMA linked list

Hello,Trying to implement SPI bus (Master only) to transmit 16 bit to LCD, utilize linked list GPDMA ch 6, I looked at the UART linked list example and tried to modify it to work with SPI with no success, only the first half word is sent and then it ...

Oyulz.1 by Associate II
  • 1230 Views
  • 3 replies
  • 0 kudos

USB field programming

Hi,   I want to start using the STM32U073KCU6 MCU in an upcoming product but don't have a ton of familiarity with STM MCUs. My attraction to the device is based around the integrated USB functionality and I am trying to figure out if it can be field ...

teva by Associate II
  • 1319 Views
  • 4 replies
  • 2 kudos