User Activity

The datasheet for STM32H723VG (https://www.st.com/en/microcontrollers-microprocessors/stm32h723vg.html) states that the devices have 2 x 12 bit, 2-channel DACs. However, in STM32CubeMX I see only one DAC listed (device = STM32H723VGT6).Is this an err...
The STM32CubeG4 package comes with CMSIS v5.6 (https://github.com/STMicroelectronics/STM32CubeG4/tree/master/Drivers/CMSIS) which I think was released in July 2019.Is it necessary to use this version or can I upgrade it to a later release? Currently ...
I can produce a sine wave using DAC1 + DMA on a STMG431CBU6 MCU, but I'd like to increase the frequency (purely as a learning exercise).  In the application note https://www.st.com/resource/en/application_note/an4566-extending-the-dac-performance-of-...
I need to generate 3 PWM signals with the same frequency and referencing the same start point (so sort of synchronised) but with different duty cycles and delays before the pulse, like this:I'm using a STM32G474CEU6 MCU and STM32CubeIDE.I've spent da...
Is there a spice model for these op amps?  I am using a stm32g474ce.
Kudos given to