STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Artuan by Associate II
  • 731 Views
  • 0 replies
  • 0 kudos

Does remap of CAN1 pins work on STM32-E407?

I bought a few Olimex STM32-E407 boards lately. I need to use the CAN1 bus. However, the default PA11, and PA12 have not populated, and I remapped to PD0 and PD1. The code always failed immediately at CAN_init (generated by STM32CubeMX). No choice, I...

schow.11 by Associate II
  • 2120 Views
  • 4 replies
  • 0 kudos

TIM2 DMA PWM to PA2 get no effect

my type is stm32f031c6. i used TIM2_CH3 binding to DMA1_Channel1 , and set in PWM1_MODE.i find the PA2 no AFIO register to remapping function. the PA2 gotta no PWM pulse.

Jseyn.1 by Associate III
  • 2411 Views
  • 5 replies
  • 0 kudos

STM32H750vb want create stldr ,I need help

I learn the lesson,but it STM32F769I-Discovery board​this video use file but i can't find it.i look this video already copy the file,add the project,is true?i guess new project,copy the file ,add project,addtion, Where there is need to modify?thanks,...

Qqixi.1 by Associate II
  • 1115 Views
  • 1 replies
  • 1 kudos

Resolved! Can not write data in flash of STM32G030C8T6

This is my code;it when run to the code in the picture, the MCU will deadvoid Flash_Test(void){  U32  Write_Addr = FLASH_USER_START_ADDR; //FLASH_USER_START_ADDR=((uint32_t)0x0800E000)  uint64_t data64=0x1234567812345678;  EraseInitStruct.TypeErase ...

Pzhu.1 by Associate II
  • 1636 Views
  • 2 replies
  • 0 kudos

STM32F407 blink project not working

I'm trying to figure out if the board is functional by trying the simple on board LED blink project, the board is STM32F407VGT6 and IDE is Keil uVision5. I'm using the code below:#include "stm32f4xx_hal.h"   void configureLEDpins(void); void msDelay(...

ATAB.1 by Associate
  • 995 Views
  • 0 replies
  • 0 kudos

Resolved! UART CONFIGURATION PIN DETAILS

Hi Team I want to interface UART on my STM32H7B3I-DK device I am aware of the code that needs to be generatedusing the ide for UART ,I am not sure on the pin connections that needs to be made inorder to receive the data Can you please let me know the...

DRAME.1 by Associate II
  • 1165 Views
  • 2 replies
  • 0 kudos