User Activity

Working with a Nucleo H743ZI2 board; after connecting the board to an external circuit I think the board was damaged. When connected via the STLink port, the LD6 light remains on and nothing else. I think LD6 indicates overcurrent. Anyone have any su...
I'm trying to determine how easily it is to switch between Nucleo controllers in the F4, F7 and H7 series, for future adaptations of a project.I noticed for a few Nucleo boards (single-core H7A3ZI, also dual-core ones H745ZI and H755ZI), there are a ...
I'm using the Nucleo H743ZI2 right now and have mostly just been using the pins accessible through the ZIO connectors (CN7, CN8, CN9, CN10). I'm wondering about the main purpose of the Morpho connectors (CN11 and CN12). I've noticed most of the Morph...
I'm using a Nucleo F429ZI and I'm using a dual bank configuration. I'm trying to make sure I understand the read protection levels. If I want a feature that allows me to save a program written into the other bank (e.g. save it to a usb as back up), i...
I'm using a STM32 Nucleo F429ZI. I'm wondering if there's a way to access the system's bootloader (not an IAP bootloader) through one of the Nucleo's communication ports (e.g. a UART port), and if this requires any hardware connections like connectin...