cancel
Showing results for 
Search instead for 
Did you mean: 

Load multiple applications to flash and pass execution from one to another

DBurr
Senior

Hi,

I'm using an STM32F746ZG and writing my own custom bootloader. The bootloader will work by initially running and determining which of 2 applications to launch, both stored at different locations in the MCU's internal flash memory. How do you pass execution on to one of these 2 applications from the bootloader?

Thanks,

Doug Burrell

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

Short answer: Do this, except use the location of your program instead of BootAddr.

https://community.st.com/s/article/STM32H7-bootloader-jump-from-application

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

10 REPLIES 10
TDK
Super User

Short answer: Do this, except use the location of your program instead of BootAddr.

https://community.st.com/s/article/STM32H7-bootloader-jump-from-application

If you feel a post has answered your question, please click "Accept as Solution".

Thanks for the fast response! This FAQ that you're referring to applies to the STM32H7, will the same solution also work for the STM32F7?

It illustrates control transfer.

You're using a micro-controller, you can pretty much test whatever memory region you want, and jump/branch into code there. On the CM7 parts this is typically done via the Vector Table. You might want to review texts on the Cortex parts, technical manuals from ARM, and IAP examples from ST

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks, yes I've done similar stuff on other ARM Cortex MCUs before and it was also through the Vector Table. I'll have a look at the IAP examples.

You can integrity check the images before transferring control. ST does some superficial tests on SP/PC, but real devices would need more rigour so you don't brick the system.

You could also copy an image stored in FLASH to RAM. You might want to think about this if you want the Apps to be interchangeable, ie keep old/new versions

The Cortex-M doesn't provide for relative addressing in the vector table, so the build address fixated by the linker is where the code needs to execute from.

If all the rest of the code is "address independent" an address specific vector table could be constructed in RAM by the loader, and you could do a simple base relocation.

If you stage the apps as object files, the loader could relocate on the fly as it commits them to specific addresses within available Flash space.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

The idea, and one I had previously implemented on another project, is to generate a build specific to a set location in memory and then generate a second build for another location. Basically have the contents of the flash split into 3 areas: 1 for the bootloader and 2 application "partitions". The problem is each "partition" requires a unique build since as you mentioned the Cortex-M doesn't provide for relative addressing in the vector table. But you're saying you could construct an address specific vector table by the bootloader. Where can I find out the specific info needed to do this?

>>Where can I find out the specific info needed to do this?

I use logical deduction/reasoning, it opens a lot of destinations, it takes longer to draw a map.

If you build for two addresses you could "diff" the binary to confirm that the code itself is "address independent". Once you've confirmed the tool settings get you there, you can build for address zero (or 0x08000000), and then you add the new base value/offset to the vector entries.

Carve a space out of the linker's RAM model, or ensure an empty "Vectors" array gets placed at the base of RAM at 0x20000000

Move the vector into the RAM table, fixing it up and set the SCB->VTOR there. VTOR needs to be on a 512-byte boundary (might be larger, check the size of vectors used, move to next binary page size)

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Piranha
Chief II

That ST's example is as all ST's code - pretty fragile and dumb. Look at my comment for a much more robust and simpler solution here:

https://community.st.com/s/question/0D50X0000AFpTmUSQV/using-nvicsystemreset-in-bootloaderapplication-jumps

DBurr
Senior

Thanks for the feedback. I've finally got HW and have been testing out the solution. I'm using the initial solution provided by @TDK​ and this seems to work, most of the time, but sometimes it doesn't and after the bootloader has run and handed off execution to the other application there's no activity and the processor appears to be dead. The solution @Piranha​ has suggested won't work for this application because it needs to determine which of 2 application partitions it should branch to and this is done by reading data from a flash chip. Anyway, I don't understand what is going on such that sometimes it works and sometimes it doesn't work. Any suggestions?

Thanks,

Doug Burrell