STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART-1 working code reads NULL

Hi clive I have interfaced UART DATA device(sender) and NUCLEOF401RE(receiver) I have set the proper BAUD RATE 115200I am using UART-1 to receive dataI generated the code in the IDE and first tested for transmit functionality and it works fineI took ...

DRAME.1 by Associate II
  • 2835 Views
  • 2 replies
  • 0 kudos

STM32F4 wake up from stop mode with UART

I am using STM32F407VG MCU (STM32F4 Discovery board) and I want my MCU to wake-up from STOP mode when it receives a message from UART. I had to adjust some things manually because the STM32CubeMX is unable to set UART Rx pin as an GPIO interrupt pin ...

0693W0000059MTEQA2.png
MKosa.2 by Associate
  • 2588 Views
  • 1 replies
  • 0 kudos

Resolved! I have an product using a STM32l486. It uses USART1 with transmit and receive DMA to communicate over a serial port. Serial port packets are all the same length. My application works in run mode, but not in sleep mode.

I can send and receive packets in run mode, but I never get a RX DMA interrupt when in sleep mode. I do not have any interrupts enabled in the USART hardware, and do have DMAR and DMAT enabled. Any ideas on what might be missing?Thank you.

Write time-out on STLink UART

Hello,I am using an STM32F072 Nucleo board. I use the STLink USB-to-UART bridge to communicate with the MCU.From time to time, the STLink UART on the PC gives a write timeout. I cannot reproduce this readily, it does not happen often.The COM-port sti...

pietrow by Associate
  • 2367 Views
  • 3 replies
  • 0 kudos

How to configure two DMA channels (ADC and UART)

Hi I'm using STM32cubeIDE and I use two DMA channels,DMA1_Channel1 is for ADC1 and DAM1_Channel5 is for USART1_rx.USART1 is using for RS485 communication. HAL_ADC_Start_DMA(&hadc1, &adcVal[0], 8); HAL_UART_Receive_DMA(&huart1, &rxBuffer[0], DMA_RX_BU...

HLEE.5 by Associate
  • 1509 Views
  • 1 replies
  • 0 kudos

Setting the Clocks on the STM32F105 for I2C

Hi allI am struggling to get the I2C up and running. I set the clocks and initialisation up in CubeMX (latest version) and when debugging the code I keep getting the pclk1 variable coming back with 1000000 which is below the limit so I get a HAL_ERR...

NCook.9 by Associate
  • 1011 Views
  • 0 replies
  • 0 kudos