Skip to main content
RBarr.1
Associate
June 23, 2020
Question

Transfer Error (invalid Data) with USART1 & DMA

  • June 23, 2020
  • 4 replies
  • 1169 views

Hello,

I setup USART1 using DMA with a STM32G071 & using HAL lib.

Currently, i try to send uint8_t TxBuffer[7]={0x16,0x07,0x98,0x09,0x00,0x00,1B}.

Transfert is done using HAL_UART_Transmit_DMA(&huart1, &TxBuffer[0], 7) and i have well manage the required interrupt signals because it send 7 bytes on Tx signal multiples times & not only ones;

but on the Tx Signal when i look the data transmitted by the DMA to USART, i can see the folowing data {0x16,0x07,0x98,0x03,0xD0,0x00,00}... 3 first bytes are always right but the other bytes values are always wrong...

It look like that DMA was badly configurate (wrong memory increment). but it seem right (see below):

hdma_usart1_tx.Instance = DMA1_Channel3;

hdma_usart1_tx.Init.Request = DMA_REQUEST_USART1_TX;

hdma_usart1_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;

hdma_usart1_tx.Init.PeriphInc = DMA_PINC_DISABLE;

hdma_usart1_tx.Init.MemInc = DMA_MINC_ENABLE;

hdma_usart1_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;

hdma_usart1_tx.Init.MemDataAlignment = DMA_PDATAALIGN_BYTE;

hdma_usart1_tx.Init.Mode = DMA_NORMAL;

hdma_usart1_tx.Init.Priority = DMA_PRIORITY_LOW;

Do you have any idea what it happens here?

Thanks a lot

This topic has been closed for replies.

4 replies

waclawek.jan
Super User
June 23, 2020

Is this reproducible?

What's your hardware and how do you receive the data exactly?

What's the primary clock source of STM32?

JW

RBarr.1
RBarr.1Author
Associate
June 23, 2020

Yes is it reproductible.

I use a stm32G071G8 mcu on custom PCB (i dont'use a nucleo board).

The data are sending out the MCU on a Tx Line & i check it with an Oscilloscope.

I have already Try a transfer Without DMA Using HAL_UART_Transmit(&huart1, &TxBuffer[0], 7,TIMEOUT) & it work well the data values are always correct.

I have also try to send a bigger buffer to check if the phenomena happens at the half of the buffer... but no, it always happens after 3 byte (it look more like a memory increment issue)

RBarr.1
RBarr.1Author
Associate
June 23, 2020

I forgot I use internal clock sources with HCLK 55MHZ

waclawek.jan
Super User
June 23, 2020

No idea.

Sounds like some FIFO-related issue (?)

Try to rewrite it as a minimal program without Cube/HAL, using direct register access.

JW