User Activity

Hi,the IPR bit assignment in 'PM0253 Rev 5 p.189' tells me that a number of bits [n-1:0] are read as zero and ignore writes.At this point n isn't 'n = m MOD 4'.Obviously n is 4 because i can write only the four upper bits and bits [3:0] stay at zero....
Hi,i have a STM32H743 with an external voltage reference with 2.5V and want to use the internal temperature sensor.When i use the calibration values from flash i converted them by ((TS_CALx *33.0)/25.0).The measured value at room temperature seems to...
Hi!I have an external sram connected to a STM32H743. It has a 16 bit wide data bus.I started a memory test and got lots of errors. So i had to look at the data in the sram with STM32CubeIDE 1.30.For example:I fill the complete memory with 0xFFFF. (no...
Hi,at the moment i'm stucked at the configuration of the MTL (STM32H743).For example:I'm looking at RM0433 rev7 p. 2934.RQS (Receive Queue Size) has only 3Bits [22:20] and 'this field indicates the size of the allocated Receive queues in blocks of 25...
Hi,i'm looking in the reference manual RM0433 rev7 for the STM32H743 on page 2910.Bits 20:18 DSL[2:0]: Descriptor Skip Length This bit specifies the 32-bit word number to skip between two unchained descriptors. The address skipping starts from the en...
Kudos from