STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC self calibration

​Hello,I am using STM32L471QE.​Please tell me how to calculate CALFACT_S and use it for ADC self calibration.I confirm that ADC1_CALFACT in CALFACT_S is 0x3A or 0x3B.I want to know how much [CALFACT_S] affects accuracy.Please let me know if there is ...

STaka.3 by Associate
  • 2858 Views
  • 2 replies
  • 0 kudos

Resolved! GPIO output is running slower than clock frequency

HiI'm trying out stm32h743 now, and try to make output signal from GPIO.I've set same frequency on F429 & H743 with same code. However, The the signal much slower(longer) in H743.F429 400nsH743 4000ns (well... my purpose is to shorten the l...

0693W000005Ci8hQAC.png 0693W000005Ci8IQAS.png
SHong.5 by Associate II
  • 1445 Views
  • 2 replies
  • 0 kudos

Resolved! Synchronize Timer 1 and Timer 8 on STM32F446RE

Hi,I'd like to run synchronous PWMs on TIM1 and TIM8 of an STM32F446RE. I use TIM2 to trigger both timers.My setup:Master: TIM2MSM bit is setTRGO = Enable bit (CNT_EN)Slaves: TIM1 and TIM8Slave mode = Reset modeTrigger source = ITR1I appended my Cube...

STM32F429 bank swap for OTA update

HiFor a project I am using a STM32F429ZITx and need to implement OTA functionality. With single bank chips I have previously put the update into the free part of the flash, then copied it over and restarted.With 2 banks I came as far as erasing the u...

CKnez.1 by Associate II
  • 1042 Views
  • 0 replies
  • 0 kudos

STM32H755ZI SPI / Proper way to receive data

Hi everyoneI'm currently working with the STM32H755ZI SPI1 peripheral. I'm using low level driver to read 2 bytes of data. I'm transmitting 2 dummy data bytes (0xFF) in order to get some response from the SPI slaves. Most of the time, the receive wor...

DSchl.1 by Associate III
  • 6872 Views
  • 11 replies
  • 0 kudos

Hi i am using nucleo L073Rz board , how do we authenticate a user application bin file flashed in to a board from iap is the correct bin and move on to run.

The problem is crc used in iap for transferring the bin file is to only check for errors during the transfer process , however i dont want any random bin files to be flashed into the flash or executed from it, only certain signed bin files need...

svii by Associate III
  • 1718 Views
  • 3 replies
  • 0 kudos