Skip to main content
DU2
Associate II
July 31, 2020
Question

how to give program to L031K6 when detached from board?

  • July 31, 2020
  • 3 replies
  • 850 views

hello, I am using L031K6 with UM1956 board.

I am trying ultra low power sensor project with it.

I would like to detach the board(UM1956) then make own circuit

in that case, how to give program to L031K6?

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
July 31, 2020

Presumably you'd need to wire back up the SWDIO/SWCLK connections, or use one of the methods provided by the system boot loader (see app note AN2606)

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
DU2
DU2Author
Associate II
July 31, 2020

thanks for answer. but when I wired up that connections and give program to L031K6 by JLINK 4 pin,

what option should I set in IAR compiler? I am using IAR Imbedded workbench IDE (EWARM 7.0) ​ with dongle.

prain
Visitor II
July 31, 2020

Make sure that you are providing VDD and VDDA to MCU. what error massage does IAR show?