STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to use the Basic Timer 6 on STM32F407 MCU.

I have to keep a pin high for a certain amount of time, about 1us, I figured that it probably makes sense to do this with a timer. I was going to use SysTick but I decided that it makes mores sense to learn the timer peripherals.I think I have the co...

JCorl.1 by Senior
  • 3503 Views
  • 2 replies
  • 1 kudos

STM32G0 DMA and DMAMUX connections

HiI'm trying to write simple code on STM32G030. I read PM and RM for this uC. I try to find where is written which DMA channel is connected to which DMAMUX. for example DMA has 5 DMA channels numbered from 1 to 5 and DMAMUX has request lines numbere...

sholojda by Associate III
  • 1722 Views
  • 3 replies
  • 1 kudos

Fail to read from Ambient Light Sensor OPT3001

Hello,I'm still able to read i2c sensors (such as the TMP75 temperature sensor, the FT6336 touch sensor, and the TCA6424 multiplexer).However it seems I'm not able to read data from OPT3001 ambient light sensor. The code is the followingstatic void ...

AMerc.4 by Senior
  • 1927 Views
  • 1 replies
  • 0 kudos

Hi, I have a problem with the scatter file

In STM32F407, I get into trouble when I write the scatter file as follows. LR_IROM1 0x08000000 0x00020000 {  ; load region size_region ER_IROM1 0x08000000 0x00020000 { ; load address = execution address  *.o (RESET, +First)  *(InRoot$$Sections)  .ANY...

Hafsh.2 by Associate II
  • 2504 Views
  • 1 replies
  • 0 kudos

Sprintf STM32L4 not work I see just 0

God moorning I trying to view the output of sprintf of float value on the terminal I/O using nucleo stm32L4.I am using IAR. but i see just 0.                char pippo_alb[20];                  sprintf(pippo_alb,"%g", 27);        In ''project options...

bfran.1 by Associate II
  • 833 Views
  • 0 replies
  • 0 kudos

Executing the main while loop every 60us

Dear ST Hello,I am implementing an infinite state machine on stm32F409 board and I have an issue.I Have a periodic pwm of 60us triggered. I Want to move all the code to the main while loop from the Interrupt service routine.My objective is to run ea...

Tsemr.1 by Associate II
  • 3341 Views
  • 5 replies
  • 0 kudos

Error Sending data to Arduino through UART Communication

Hi, I would like to send a data from my STM32F401CC to Arduino. I have connected Tx to Rx and successfully upload the code to stm32 and Arduino Uno. I don't get the values right, only first four readings, then all the values become random. This is my...

0693W000007DOgyQAG.png 0693W000007DOgGQAW.png 0693W000007DOifQAG.png
Malre.1 by Associate
  • 2691 Views
  • 3 replies
  • 0 kudos