User Activity

environment:STM32CubeIDE Ver1.6.0Thank you for helping.How do I add image compilation options?Thank you.
Thank you for your help.I'm a beginner.The following function is called by the line interrupt, but swapFrameBuffers () seems to be empty.Specifically, what kind of code should I write?What should I refer to and how should I switch between the two add...
LCD_CLK that runs XGA (1024 x 768)Thank you for helping.environment:STM32CubeIDE Ver1.5.0MCU: STM32F769BIBoard: CustumIt seems that this microcomputer supports up to XGA, but LCD_CLK for XGA is not output.Create LCD_CLK with PLL using a 25MHz crystal...
Thank you for helping.environment:STM32CubeIDE Ver1.5.0TouchGFX Ver4.15.0Board: CustomMCU: STM32F769BIOutputs RGB parallel signals from the MCU.I want to output a 65MHz LCD_CLK, but the LCD_CLK signal is not output.Why?The transmitter is 25MHz and Sy...
Thank you for helping.If you create a project with STM32CubeIDE, it will be included as shown in the image below.Where is this set in the IDE?